Posted on April 21, 2015 at 18:20Dave,With regard to the error code 02 which is a VCEL watchdog test failure error, the VCEL errors usually occur when there is a hardware issue. If you send me a copy of your schematic and layout to mailto:kenneth.w...
Posted on March 26, 2015 at 16:33Thomas,The maximum functional operational voltage is 3.0V. Running the device at higher voltage is not suggested. It will not operate according to the specified operation parameters. The absolute maximum value f...
Posted on March 26, 2015 at 15:29Tim,Sealing the vent hole will not negatively affect the operation of the part, but it may cause some issues during a reflow process due to pressure build up from the heat. Even with the vent holes sealed the package...
Posted on March 16, 2015 at 17:29I would like to test your code on a STM32 Nucleo board and satellite I have. Can you supply a document on how you have it connected? Since you are not seeing any communication on the I2C bus, have you checked the p...
Posted on March 09, 2015 at 20:28A ranging error of 1 is caused by a failure of VCEL continuity test. This is can be caused by: 1. AVDD_VCEL (pin not connected well and powered by 2.8V. 2. AVSS_VCEL (pin 9) not connected to GND 3. An internal pro...