User Activity

What pins should we use if we would like to interface with the BlueNRG-M2SA module via UART. We currently use a UART interface on an older competing Bluetooth module and would like stay with that communication interface instead of SPI which is used o...
Can the combined PWM signal be the AND of two reference PWMs in which one is negated?This is what I would like to do. Combined PWM signal = OC1Ref AND NOT(OC2Ref)If I could set the polarity of the two reference PWMs differently, I think that would ...
We are laying out a prototype board with the ISM330DHCX in which we would like the option of using the part in Mode 1 or Mode 2. The board will have zero ohm resistors that will allow the other sensor to either be connected directly to the ISM330DHC...