I using stm32F4 discovery board. I am having issues with the ADC. The voltage signal changes after I give that signal as Input to ADC. This may be because if leakage current of Analog Pin. Can you guys suggest the way-out from this. RegardsMusab
static void MX_ADC1_Init(void)
{
/* USER CODE BEGIN ADC1_Init 0 */
/* USER CODE END ADC1_Init 0 */
ADC_ChannelConfTypeDef sConfig;
/* USER CODE BEGIN ADC1_Init 1 */
/* USER CODE END ADC1_Init 1 */
/** Configure the global featur...