User Activity

Hi All,I've had some logging code written some time back and I'd like to be able to selectively prepend the date/time onto what gets passed in however I'm at a loss as to know how to do this or where to start. The code that was supplied is below.#if...
Hi All,I'm using the following code to set up 4 external triggers and this all works well. What I'd like to do is to be able to change the trigger type of any of the EXTINT at some point in the program. I've tried a couple of things which only resu...
Hi All, I've created a PCB (same happens on the Open107V dev board) and I'm finding that the I2C comms is failing unless I have an external capacitor of 22pf connected from the SDA line to ground. I know the aim is to keep the capacitance as low as ...