The project works on the B-G474E-DPOW1 Discovery kit. I have searched the instruction about the joystick on the board and with an oscilloscope I have seen the Automatic and Manual resistor load selection. The LED's on the board flashing as expected.I...
After some test I have found this way for compiling the project:I have selected the button Start new project form STM32CubeMX file (.ioc) Then I have selected the file PSU - Buck VoltageMode_HW G474inLQFP64.iocThe file is at the following path:C:\Use...
I have the B-G474E-DPOW1 Discovery kit and I have downloaded the Buck_VoltageMode_HW project from ST repository. I build the project without error and it runs as expected.After double click on ioc file the ST32CubeIDE suggest me to migrate to MX ver....