User Activity

Using CubeMX 5.3.0 to autogenerate a sample STemwin example set of code for TrueStudio seemed to work well. It was created choosing the STM32F429 Disco board and adding the STemwin graphics options...no customization of any settings was done. The p...
Hello,I'm looking to use the STM32F429 to output data to an SVGA display. The supported video formats for the display are shown in the image below. The display is actually a monochrome variant, so color is not relevant as the RGB lines are tied tog...
Hello,Using the MCSDK monitoring tools, we have been able to drive our motor up to 6000 RPM with no issues when unloaded. However, when we put the unit under load, then the desired and achieved RPM deviates somewhere around 4000 RPM. The system is ...
Hello,We have used your MCSDK successfully in a custom BLDC design and it is working well. We have some conditions however when we are reducing speed on a large inertia and this causes an overvoltage spike. The MCSDK faults on this (we have it set ...
We are using the ST MCSDK, it is very helpful. In MCSDK/MCLib/Any/Src there is a function called STM_FaultProcessing. It is auto generated by Cube. We have one line we want to add to it that turns an LED on alerting the user to a problem. This wo...
Kudos from