Thank for this answer. It seems to imply that you are comfortable with attaining normal refresh rates for display of 1024x7689 or below, and that resolutions above that up to the 2k+ pixels allowed by the register sizes may or may not work as the int...
For anyone else getting similar SD card issues with DMA I thought I'd share that it can work. I'm using v5.0 of CubeMX and can confirm that the SD card is working on my STM32F769 discovery board. In MX, you've got to enable DMA for RX and TX as well ...
ST now has a number of discovery and other boards with USB HS OTG/Device (either with external or internal PHY) and all examples seem to be the now very old USB Audio Class 1.0. Hopefully UAC 2 will be forthcoming, and since at least two boards now h...