User Activity

Hi!!Do you know any adapter from lqfp144 to DIP format so you don't have to solder in SMD?Thanks.
Hello, I look for solutions for a problem that I have.I am designing a USB-OTG stage for the STM32F469ZIT6 microcontroller.What I'm looking for is that through a pendrive with standard type A connector can automatically load a .bin application.The pr...
Hello, I have this design but I think the clock does not rock me. How can I check it without having an oscilloscope? I have a voltmeter but I measure the voltage at both ends and it varies only between -100mV and 100mV ...I have made a bootloader to ...
Hello!I am trying to program a bootloader so that it loads directly my application (.bin) through the USB in the electronic card STM32F469-DISCO but it does not work for me. I would like to know if there is a generic bootloader that I can download to...
Is the design of this circuit OK to be USB HOST?https://drive.google.com/open?id=1zKJQuh5CJrl1X4RY4lJzdEwwPDz0wLm2https://drive.google.com/open?id=1pBKWj9IoOnVFrW1I-eUM-54Y8_F0gw5J