User Activity

Hi,We are using LIS2DH12TR accelerometer sensor in our application. Attached is the circuit for the same. We are using a P-channel Mosfet part# BSS84W-7-F to switch the sensor on/off. We are able to switch On the sensor through the Mosfet but we are ...
Hi,We are using STEVAL-ISA136V1 for our application. We need +3.3V, 0.6A output instead of +5V, 0.6A as per STEVAL-ISA136V1. Let me know what value changes in feedback resistors are required or if any other changes are requiredRegards,Kamesh Lakhwani
Hi,We are using STEVAL-ISA140V1 for our application. We need +15V, 1A output instead of +12V, 1.25A as per STEVAL-ISA140V1. Let me know what value changes in feedback resistors are required or if any other changes are requiredRegards,Kamesh Lakhwani
Hi,We want to know is there any Air quality sensor available in STMicroelectronics ?.The host controller that we are using is STM32L462CEU6. Also, Please let us know how can we interface this Air quality sensor with STM32L462CEU6 asap.Regards,Kamesh ...
Hi,We want to use IMP34DT05 Sound sensor in our application.The host controller that we are using is STM32L462CEU6. Please let us know how can we interface this sound sensor with STM32L462CEU6 asap.Regards,Kamesh LakhwaniProject LeadSystem Level Solu...