User Activity

Dear Support, in the data sheet of LED2001, it provided the layout reference, but it didn't mention the copper thickness. for the demo board, what is the copper thickness in oz of the PCB of.STEVAL-ILL054V1,  Thank you very much, David 
Dear Support,I have a design which works fine even drive it full PWM with 0.025 ohm (4A max current). we need to control the backflow current so added a diode on the power supply path.  the schematic is attached. C169 and C170 not installed. it works...
for LED2001, the marking on the chip like LED2K1xxxx118. or xxx125. how to understand the Marking under the LED2K1? Thank you,David
Dear Support/Expert I have a question about LED2001, is it practical to apply a relay to switch the LED off, but keep the DIM enabled.  as in the schematic. if K21 is off, it will cut the current off of the output, but the DIM pin of the LED2001 is s...
Dear Support and Expert, We are using LED2001 to drive a LED, 2V@4A. the 6 boards come back. 4 work good but 2 no output voltage. we are using QFPN package, is there a way to check the pins are properly soldered beside take it out and reinstall? 2. i...
Kudos given to