the note says this: The STM32L microcontroller on the board is not intended to be programmed by users. ST provides a preprogrammed firmware image for the sole purpose of interfacing BlueNRG-1, BlueNRG-2 to a USB host device.
I saw that is possible using a SSD driver and specific functions to drive it by serial port. Could i load the txt file on an ssd and than the MCU could access to the txt by serial port. Is this a good solution?
thank you. I had already seen this document. The problem is that the power to which these devices transmit is not indicated, therefore with the measured RSSI value, I cannot get an idea of how far and intensely these devices are able to transmit. I...