Hello Martin,I did a quick change for 24Bit depth and it seems to work well. Using the internal Portrait functionality together with this mirror provides the 270 degree that I need.Please find the updated Code attached.Daniel
Hello Martin,I would be very pleased if you can provide the source. Support for 90, 180 and 270 degree is really useful for the discovery boards since the rotation in the projects is mainly selected depending on the connectors. I'm currently working ...
Hello,is there already some progress to this topic.I'm just rewriting an application from emWin to TouchGFX which is using a Stm32f746 Discovery board in portrait orientation.All mechanics are fixed and the units are already in use with current emWin...