RESOLVED: Changed the end node to use US915_HYBRID, turn off Automatic Data Rate (AT+ADR=0) and set the Data Rate to 4/5 (AT+DR=4). Set Gateway to receive on sub Band 1 which is the lower 8 125kHz channels. This also set the Spreading factor to 10...
HI, yes, that I have, the US915 contains 64 125kHz wide channels. However most Gateways only receive 8 of those channels within each sub-band, of which there are 8 sub bands within US915, Most Gateways allow us to select which sub-band to use, for ...