User Activity

Helle everyone,I want to use the littleFS file system library that I used in my previous projects in STM32H753 Internal Flash Memory. But the fact that the block size in STM32H7 is 128K made me think a little. I normally use littleFS on 1K blocks and...
Hello everyone,I want to develop a project for STM32MP1 using stm32cubeIDE Version: 1.15.1. In the yocto-related part of the topic, I successfully compiled a kernel and produced an SDK for the relevant kernel. I want to import this SDK into the cubei...
Hello everyone,I'm getting yocto build for STM32MP1 mickledore. There is no problem with compilation. The images were produced without any problems. The system is up but I get the following error while generating the SDK.   ERROR: core-image-minimal-...
Hello everyone,I got a yocto build from scratch using yocto/open-embedded/meta-st-stm32mp. Everything is smooth. I can root the kernel while standing. I can establish an ssh connection. Everything is perfect.But I want to create an SDK after the kern...
Hello everyone,I made a yocto based build using stm32mp1. After compiling, I followed these steps: I created 5 different partitions in the SD card. These are as follows.  I uploaded the following files to the partitions I created, respectively.sudo d...
Kudos from