User Activity

I use ST25DV to write binary files. I can only write one BLOCK at a time. I think every time I write is Multiple BLLOCK,Each BLOCK has 4 bytes. If I want to write 64 bytes(binary fules), the boad have to read and write 16 times. If I want to read and...
There is a Spiral antenna in the X-NUCLEO-NFC04A1. The link is https://www.st.com/content/st_com/en/products/ecosystems/stm32-open-development-environment/stm32-nucleo-expansion-boards/stm32-ode-connect-hw/x-nucleo-nfc04a1.htmlBy the document AN2972(...
    my reader is st25r3911b-discover,the tag is st25dv04k,when I write file(the bin file )to tag,the reader wrote a block (four byte)to tag every time ,how to designer reader for writing more block to tag every time.for example two block or more.than...
I use pc software(ST25R3911B Discovery GUI) linking with ST25R3911B in usb.the tag is st25dv04k.My order of operations is | ST25 Tag Editor model | > | ISO15693 model | > | DYNAMIC NFC TAGS| > | ST25DV04K|.I use file transfer model,choice LOAD FILE T...