Is there any user guide regarding custom board creation in MC workbench 6.1.0? I can start from the X-NUCLEO-IHM05M1 board, but I have to change the HALL sensor input from TIM2 to TIM3.
I am using the latest motor control workbench (6.1.0) and the CubeMx (6.6.1). The motor control code generation is working if all the files copied to the project folder. If I select the "Copy only the necessary library files" some header files will m...