User Activity

Hi everyone,I have a question about MCSDK for STM32G474QE mcu.I chose STM32G474QE in MCSDK gui software. My hardware phase sensing pins are connected to ADC1_IN5 (PB14) and ADC1_IN15 (PB0) pins. I want to use these pins for 2 insulated current sensor...
I am using the stm32g474rct6 RTC module. over a duration of 2 days, the drift was over 15 seconds. I tested it in standard room conditions. How can I solve this problem ?
I want to make custom stm32WL board layout with antenna path. I found NUCLEO-WL55JC. This board has BGA package for stm32WL55JC.Q1: I need stm32WL QFPN package board layout and antenna path. Is there board layout and reference design for stm32WL55CC ...
I am working with ST-MotorControl Workbench. I generate the project according to 72 Mhz clock with WorkBench. I can't choose 56MHz through WorkBench. So, I re-generate project for 56 MHz with CUBEIDE. And than, I edit the code (picture). Is there an...
I try to drive (FOC) BLDC motor with STM32G474RE MCU. I use a custom board. I use INA240A1 for inline current sense. Can I use 3 shunt inline current sense method for ST mcsdk ? In STs evaluation boards typically low side shunt resistors are used for...
Kudos from