So,is my idea right? The LPUART can not use LSE to configure BaudRate 9600?The error values in RM0377 are Wrong?Can you provide the actual error value when configure BaudRate 9600?Regards
I tried.The value of BBR is set to 0x0036a.When the baud rate is set to 4800,The value of BBR is set to 0x006d4. And actual BaudRate is 4672,The error is less than 3%. 32768 divided by 7 is 4681.So,the error of 4800 is small.As shown in the figure b...