Posted on April 30, 2013 at 11:53
Hello,
I would like to use the internal microphone built in the board to hear the sound from headphone jack in real time. After that I 'll be implementing filter to the sound but thats not so important at...
Posted on April 30, 2013 at 18:33
Thanks for the reply. 16 kHz is the sampling rate actually. The array is filled with 440 Hz sine wave which I extracted from a wave file. The duration is 250ms.
I usedEVAL_AUDIO_TransferComplete_CallBack ...