Hi,I'm using a Nucleo -F303RE with X-08 inverter board, and need to enable the SPI peripheral.Code is built directly from the ST MC-SDK 5.4.4, (FOC mode) then examined in Cube-MX 6.0.1. Built in Keil uV5 - no change to project options given by MC-S...