User Activity

For evaluating the WB55 i would like to have software on a PC that can accept data from the Nucleo board over BLE. Since my PC doesn't have the latest Bluetooth version i want to use a WB55 as the radio. Zephyr RTOS has an example that would make the...
I tried flashing PWR_STANDBY_RTC and PWR_EnterStandbyMode examples both has sleep current of 590uA. How do i get the datasheet value of 600nA standby current or atleast something less than 10uA.
My application only needs to send data once every few minutes during which time i can save power by turning off the radio. I don't see any examples that do it, they don't even have a deinit function.
With the throughput example if i use 2 WB55 boards, the maximum throughput that i get is 2KBpsDT = 2160 bytes/s lost = 0If i use my phone with PHY1, i get 90KBps+ and with PHY2 sometimes its 150KBps and sometimes 15KBps, on download. With upload its ...
I followed this[1] URL to update FUS and wireless stack, it failed and now i can't get wireless to work. All the examples are hard faulting. My FUS is still in version 0.5.3Reading 32-bit memory content Size : 4 Bytes Address: : 0x2...