User Activity

Hello all!We are using L6470 in our product for stepper motor control. We are using the SPI mode control with MOVE command.I would like to know the time (relative to given external clock) it takes to run the motor for given distance, given max speed ...
Hello!We have custom board build with STM32F427 and embedded linux and i am trying to connect the STM32 bootloader with canbus. On the board the STM32 uses CAN2.I can toggle the pins BOOT0 and RESET from the linux, and i can program the stm32 fine wi...
Kudos from