I use a RGB to LVDS conversor, but i have an other question, I want to use the BSP library from STM32F429 discovery which have a tft. So the BSP use the code of the ili9341 (ili9341.h/ili9341.c) device, I know I should rewrite the part where are the ...
Hello, I want to use the same STM32 MCU to controll a TFT with LVDS interface, so I don't know how I should connect the TFT pins into the MCU. There are a MCU that have a LVDS pins that connect directly with TFT or I need a Converter of LVDS to RGB c...