User Activity

Hi friend,I want to extend the HS_STARTUP_TIME for BlueNRG-1. What is the maximum value of HS_STARTUP_TIME for BlueNRG-1? I saw the datasheet AN4494 it says that "XTAL_startup = XTAL_startup_measured*1.2*1.1*1.3 = 1.716*XTAL_startup_measured".  So 19...
Hi friend,I want to extend the HS_STARTUP_TIME for BlueNRG-1. What is the maximum value of HS_STARTUP_TIME for BlueNRG-1? I saw the datasheet AN4494 it says that "XTAL_startup = XTAL_startup_measured*1.2*1.1*1.3 = 1.716*XTAL_startup_measured".  So 19...
Hello friend,I programmed a blueNRG-1 MCU using ST Link V2. But I need to use BlueNRG-1 ST -Link Utility's application to erase MCU and need to pull up a pin (for SWD program). Then unplug the ST link V2 and plug it in. Release the pull-up pin and us...
Hi friend,I have an old project using blueNRG-1 and the ble stack used is libbluentg1_stack.a. I would like to know which version of the BLE specification is supported? Thank you in advance.Best wishesTed Wu
Hi friend,I want to implement watchdog function at Ble_beacon project of the BlueNRG-1_2 DK-2.5.0 platform. Where I need to call the function of WDG_SetReload to reset the watchdog timer? My project has I2C slave and HAL_VTimerTimeoutCallback. Thank ...