Posted on May 17, 2011 at 12:48I have an encoder interface setup, using the auto-reload to loop around for the CPR of the encoder (i.e. 0-799). Can the timer(s) be setup to give an underflow/overflow to chain to a longer (32 bit) reading. Or can the...
Posted on May 17, 2011 at 12:45I'm using the USB Virtual COM Port and noticed that there is no flow control from the PC to USB. If you type things into HyperTerminal everything works fine. But if you send a text file (a few Kb) then it gets corrupte...