User Activity

i need to measure force of a motor but i don't know i how to measure .please any one help me i'm using 24v dc motor with encoderand stm32f446re controller
im using stm32f4 series controller controls the BLDC motor.the motor control the sliding door .now i want to calculate force of door?what to do now . any suggestion??
Im using stm32f429 controller,now in our project i want to play audio in wav format.now sd card read function working fine,data transfer from uc to DAC using i2c DMA mode.but now only noice is play.what to do now ?any suggestion ?
i am using stm32f207ve microcontroller ,im receiving continuously data from another controller using 50 buffer using interrupt, after the 50 buffer is filled then again the data not receive in buffer 0 ,what i do now????
I would like to use SDIO with 1 bit mode with FatFS. I use STM32F207VE MCU. The SD card is a 16 GB SanDisk.Version of STM32CubeMX is 6.1.1, firmware version is STM32Cube FW_F2 V1.9.2.FATFS R0.11 version used.When I generate SDIO with 1 bit mode it is...
Kudos from