Posted on May 17, 2011 at 12:28I posted two questions, one about Virtual COM Port, the other about code space. The page says each received a reply, but these replies are not displayed. Please! I would really like to see the replies! I need the help!...
Posted on May 17, 2011 at 12:28We are migrating to the 32-bit world from the 8-bit world (8051), where we fit our functionality comfortably into 64k of code space. How much code space do I need for this 32-bit chip for the same code? Might I need 25...
Posted on May 17, 2011 at 12:28Aren't pullup and pulldowns done internally on the STM32F103RBT? I am looking at the STM32F101xx and 103xx Tech Ref Manual RM0008 page 75. http://www.st.com/mcu/familiesdocs-110.html#Reference%20Manual How are the GPIO...
Posted on May 17, 2011 at 12:28That's exactly how this is playing out. I just downloaded the CD-ROM files for the STM32-Primer, and found these extra lines in hw_config.c in the Virtual COM Port project: /* Configure USART1 Rx (PA.10) as input float...
Posted on May 17, 2011 at 12:28Thank you for the reply, lanchon, and I will save this circuit diagram for future reference. When I disconnect and reconnect the USB connector, I believe that the only thing that happens is that the PC detects a voltag...