Posted on May 17, 2011 at 09:59Dear All, Can anybody give me linker script for compiling code for STR912FAW46(1MB Flash) and STR912FAW47(2MB Flash). Please Help Thanks & Regards, Sachin D. Bhujbal.
Posted on May 17, 2011 at 09:59Dear All, We are working on STR912FAW46(1MB Flash) and STR912FAW47(2MB Flash), so we need IDE &(or) Compiler for it which are not in latest version of Anglia. If anybody knows latest version of Anglia for this chip, ...
Posted on May 17, 2011 at 09:58Dear All, Can anybody tell me, what is use of GPIO_IPInputConnected_Enable ? When this to be enable or disable ? Does it mean if a pin is Input Function pin then above property of pin should be enable or if it is Out...
Posted on May 17, 2011 at 09:58Dear chandrakant.bhor, I also using same MicroC., I also tried its RTC. Its initialisations was as follows. In following example I have used Alarm Interrupt & it was working fine. I think You are not initialised RTC...
Posted on May 17, 2011 at 09:58Thank You, VincentC, Now I am able to programme & boot required bank if I programmed those from Rflasher. :D I downloaded my Application in Bank0 through JTAG & after that ST IAP driver in Bank1 ( with booting from...