I've used the End_Node example in lrwan cube 1.2.0. I've only changed commissioning.h file with my network parameters. I've also tried to disable duty cycle and ADR but sending data after OTAA doesn't work. Only ABP works.
I've the same issue with End_Node project with L072z-LRWAN Evaluation kit and ttn.With ABP activation works. End node transmit and receive messages.With OTAA activation end node joins to the network, but confirmed and unconfirmed messages aren't re...