Posted on May 17, 2011 at 12:36jj, I've tried different data-transfer rates and it is the same, my problem is not connectivity (I think) but that I can't verify that my file has been successfully downloaded.I was using blinky to isolate the problem ...
Posted on May 17, 2011 at 12:36Hi, I'm using this new V1.1.1 Flash Loader, it works fine with the user interface but I'm having issues when I try to program from the command line. I'm using the KEIL MCBSTM32 demo board which comes with the STM32F103...
Posted on May 17, 2011 at 12:21Hey just for reference... I've been dealing with the same question, I wanted to setup my SYSCLK but I didn't want to use the ST firmware and was looking for the SYSTICK configuration register. I found it in the ARM web...