Hello,There is always channel 0 sampled after the chip enable by CS pin. After that you program channel to be sampled and next reading is done on that channel.Chip is almost completely disabled without CS so it doesn't remember previous setup.The inp...
Dear Dieter, can you specify which evaluation board do you use? Is it STEVAL-CCA023V1?Regarding to input voltage range. The maximum range is 70mVrms (see table 5. in datasheet) so sine signal 1Vpp is certainly above this value. Please note that sign...
Hello, Do you use eval board or your own PCB? Possibly can you share the schematic and how do you set the gain? (by resistor?). It would be also helpful to get oscilloscope traces when working correctly and when failing.
Hello Dan, Thank you for your notice.Mentioned table states 1uf for ST232E and 0,1uF for ST202E which is correct.But you are right for capacitors designators. C5 is just decoupling capacitor and table should mention C1 to C4Best regardsST support