Hi Ulysses HERNIOSUS I wanted to simulate slave cards using ST25R3916: most of the commands are standard ISO14443-A, but interspersed with non-standard commands
HI Brian TIDAL (ST Employee)There are some non-standard protocols in the beginning and transmission of a command;Most are still standard ISO14443-A, including collision prevention;I'm sure it's ISO14443-A modulation;