I have some widgets on top of an image. Those widgets have interactions defined on them. I override handleGestureEvent in my View class.It's almost like the widgets swallow/prevent the gesture event from coming through.
Only if they want Keil to flash it. I have no issues with mine (it is flashed separately to Keil to speed download speed). I still specify the section and it works fine (just doesn't program it).
My apologies - you're right - I didn't realize that. Has this debugger you're using worked before? You mentioned it's an ST Link clone; maybe it's not playing well with the driver.Another option is trying it through Cube IDE - it's good software. I'm...
I did not, I do not have an H743 available. I believe the issue is related to something in the stack of Keil's loader and the debugger. I would venture that it is not TouchGFX per-se though that is your source of error.Did you try loading your outpu...
10.10 - with recent firmware and drivers. I'm loading an F769 with it. Can you get it load using the ST provided flashing utility? For Keil - what you did (remove the region from the "Flash Download" tab) worked for me. Though, our setups are differe...