Hi, allI have a project using a STM32F103c8t6 that works perfectly with HAL 1.4.0, but when I update a HAL to 1.6.1 version, the i2c device which is configured as a slave, after some writing or reads from the HOST it keeps the SCL in LOW, causing acc...