I'm using Windows 10 and arm KEIL IDE along with STM32F407G-DISCOVERY board. I'm a very beginner and trying to do something with LED. I'm stuck at the initial stage itself. I have a problem with the LED API in the Board Support Package in the set...
Thanks for the response. It doesn't do anything just simply remains as it is. At other other places while I was doing setup process when there was Yellow colored check mark and when I clicked on Resolve, it then fixed the problem automatically ...