I'm referencing to STSW-IMG009 and specifically function VL53L1X_SetInterMeasurementInMs(uint32_t InterMeasMs)What would be the maximum size of the argument and the value of ClockPLL. I'm re-writing for another platform.Regards/Claes
first question about initiating const from adr 0x2D to 0x87, is not the internal addresspointer incrementing ?Second: The default device address is 0x29 or ?(datasheet says 0x52)