As @EMECH (ST Employee) says, this is correct. The remote provisioning specification should first be agreed at the SIG and then an IOP (IOPs more likely) done to verify that this works according to specification, then the specification is released. ...
@PUrsu.1 Would you consider using the PWM to generate the DMX512 signal ? there seems to be a lot of timers on the STM32F407 which can be used for PWM outputs
Apologies for the delay, I did not notice the reply, if the statements are not coming out on terra term then we need to check the where the logs are being directed in the lighting demo project.Check the code for 1, logs are enabled 2. Which UART or ...
If you really don't want the phone to do the provisioning, the only real solution would be to wait for the ST implementation of remote provisioning, this will enable you to provision the entire 500 nodes from a single stationary provisioner. As @EMEC...
That is good to know. I would typically setup at test bed to verify the throughput and performance for the mesh to get better control on this and understand the performance envelope. Hopefully ST will also release this data on a per-release basis (on...