The intermeasurment time includes by definition the Timing budget. In theory, they can be equal but to be safe, few µs delay might help. I propose you 200ms because I thought you wanted a 100ms measurement every 100ms. That's good you found the issu...
Hello,Unfortunately, you cannot use the ULD API of the L1X with the L3CX sensor. Even if they have similarities, there are dead-end difference to prevent such compatibility.Best regardsDominique Loyer
Hello,I looks like your device is not well initialized or you have an HW problem. Did you test it at 30Hz? Which API are you using, ULD or the full version?Best regardsDominique
It's one of the difficulty of this sensor which has to be Laser safe Class1, The laser fires a limited number of photons and the sun not, even at 940nm. From a software point of view, the SHORT distance mode is the best against ambient light.Opticall...