Hi,I I am stuck in my project, I have to activate the physical sim card.the documentation says you need "Set pin Sim_select0 to low to select the plastic SIM" but I don't know how to do it.
I recently bought "P-L496G-CELL02" and I would like to communicate in AT command with the module:here is the message that appears:Welcome to STM32-Cellular to Cloud (STM32-C2C)AT commands terminal: connection to PC with USB-OTG FS is needed.Modem is ...
i solved itto activate the AT commands, you must: check the correct position of the jumpers:JP3 -> ARD_V5_INJP4 and JP5 -> + 3V3 JP 6 -> positoin 1-2 (to the left)JP7 -> STLK JP8 -> closed JP9 -> open- Open gtkterm or other similar utility and set th...