Hello,I'm currently using the following setting for the ethernet0 in Linux 5.7.6:ðernet0 {
status = "okay";
interrupts-extended = <&intc GIC_SPI 61 IRQ_TYPE_LEVEL_HIGH>,
<&intc GIC_SPI 62 IRQ_TYPE_L...
I also suspect it's the clock but didn't make any other considerations.On my machine the PHY is a KSZ8081 with a 25MHz clock interfaced with RMII. Under Linux everything works fine so I exclude hardware problems.Ciao,Rodolfo