Ocebe.1
Associate III
since
2020-11-07
2023-10-09
User statistics
14
Posts
1
Solutions
0
Kudos given
1
Kudos received
View all badges
STMicroelectronics Community
About Ocebe.1
Options
Report User
User Activity
Posts
Replies
Hello, how can I write start,stop,address and write functions for I2C Master Mode in stm32g031k8
2021-04-08
Hello, In my project when program come to this "_HAL_UART_ENABLE_IT" ,hard_fault happened What is the problem ? or what are this code ? Are there anyone help me please?
2021-03-30
Hello,I use microphone and When I talk I get the data from microphone to eeprom.I want to playback to speaker from eeprom .I think,I have to produce analog signal.But I shouldn't use DAC .How can I produce Analog signal without DAC in stm32 ?
2021-01-10
Hello,I have stm32g031k8 and I want to write and read on eeprom with registers.How Can I do that
2020-12-30
I have atmel 24c512 eeprom ,How should I do connection between board and eeprom .
Hello , I want to connect boot0 and 3.3V for reset my chip .I find boot0 pin is in PA14 but I cannot see on my board, could you help please (my board is stm32g031k8)
2020-11-08
View more
Re: Hello, how can I write start,stop,address and write functions for I2C Master Mode in stm32g031k8
2021-04-08
Thank you for your advice , I wrote a code for printf()
Re: Hello, how can I write start,stop,address and write functions for I2C Master Mode in stm32g031k8
2021-04-08
I looked these examples but it used HAL Library and I don't want to use HAL , but thank you your response
Re: Hello, how can I write start,stop,address and write functions for I2C Master Mode in stm32g031k8
2021-04-08
Thank you, I will look.
Re: Hello,I use microphone and When I talk I get the data from microphone to eeprom.I want to playback to speaker from eeprom .I think,I have to produce analog signal.But I shouldn't use DAC .How can I produce Analog signal without DAC in stm32 ?
2021-01-10
In the PWM ,I can change duty cycle and frequency but I think ,I have to change amplitude
Re: Hello,I use microphone and When I talk I get the data from microphone to eeprom.I want to playback to speaker from eeprom .I think,I have to produce analog signal.But I shouldn't use DAC .How can I produce Analog signal without DAC in stm32 ?
2021-01-10
How can I change PWM'S amplitude?
View more
Kudos from
User
Count
Legacy member
1
View all