I used X-NUCLEO-53L5A1 + 2 VL53L5CX-SATEL, and the data read output speed has a delay in the code: HAL_Delay(POLLING PERIOD), POLLING PERIOD == 1s, and then I want to quickly, so I canceled HAL_Delay() (Picture1), But it took a long time to check (Pi...
I have SPC58EC-DISP,now I use sample code(Network Gateway Test),it's MII mode and working; then,I want to use RMII mode,I set PHY MODE = RMII,it's not working, how to do it?ps:The OSC is changed to 50MHz,and SB5 Close & SB6 Open.
Hello!I have a SPC58EC-DISP; I set the PWM frequency 20KHz and duty cycle 1%,then it's not output,when set 8%,it's output 2us time;I found that the minimum PWM output time seems to be 2us.now I want PWM frequency 20KHz(50us) and 1%(0.5us) ouput,wh...
Hello Erwan,I know how to solve this problem,In low level drivers,set eMIOS0 internal counter frequency to max(eMIOS0 global prescaler =1).Now, I have another question,in the SPC58EC clock tree : EMIOS_CLK is 40MHz(Default),if i set it to 80MHz,then ...