Posted on March 27, 2018 at 14:01After some tests, it seems that when I stop all comunications with the other SPI device (same bus), the LIS2DH12 stops enterring this weird state.Perhaps there is something like data transmitted to the other device i...
Posted on March 15, 2018 at 18:20We're using SPI (MOSI/MISO/SCK/CS).VCC is 2.8VThere is another device on the bus that is driven with another CS line.Of course, we designed the code so they never ever talk together at the same time.Also, values clos...
Posted on March 11, 2018 at 17:57I'm currently using the LIS2DH12 and facing a similar issue.But instead of reading values close to 0, I'm reading fixed values that does not change when rotating or shaking the device.Here too, the power cycle manage...