User Activity

Posted on July 10, 2018 at 21:18Hi,I am using the USB VCP to connect to a PC serial window. I have connected using PuTTY, correctly received messages from the Nucleo, and correctly sent messages to the Nucleo from the window and I could see those in...
Posted on July 04, 2018 at 21:03Using TIM1 Channel 1N and Channel 2N, where Channel 1N is used for PWM output and Channel 2N is used for Toggle output, the Toggle output polarity is inconsistent. I stop both timer channels (HAL_TIMEx_PWMN_Stop and H...
Posted on June 20, 2018 at 19:10Hi all,I'm using the HAL drivers and STM32CubeMX to generate DMA Burst transfers from memory to TIM1 in OCToggle mode on the Nucleo F722ZE.Old versions of the HAL drivers had a function called HAL_StatusTypeDef HAL_TI...
Posted on June 20, 2018 at 19:00Hi all,I'm using the HAL drivers and STM32CubeMX to generate DMA Burst transfers from memory to TIM1 in OCToggle mode on the Nucleo F722ZE.Old versions of the HAL drivers had a function calledHAL_StatusTypeDef HAL_TIM...