My program is as described in stm8s reference manual 17.4.3 External clock source mode 1and pulse counting is done in pin PC7 using HSI 16 Mhz , but the speed of counting is very low , for example for a 10 mhz pulse in 1 ms TIM1_CNTRL counts to...
Posted on December 17, 2017 at 21:26I want to use stm8 mcu for electrical relay such as trip relay and must pass the esd and emc test . Which one is better to use for this subject ?I thought stm8a should be better because it will be used in automoti...
Posted on December 19, 2017 at 22:35Thanks for your reply I also use relay to generate noise. My system works with 110 volt dc.I connect the 110 volt relay coil to power supply through normaly close contacts , in this case relay will become on and o...