Browse
STMicroelectronics Community
FAQs
Sign In
Product forums
STM32 MCUs
STM32 MCUs Products
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
STM32 MPUs Products
STM32 MPUs Boards and hardware tools
STM32 MPUs Embedded software and solutions
STM32 MPUs Software development tools
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive and Transportation
Automotive MCUs
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
YLich.1
Associate II
since
2020-10-15
2023-06-14
User statistics
3
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About YLich.1
Options
Report User
User Activity
Posts
Replies
Hi , I use ST micro controller: STM32H743VIT6 1. I want to knew if the I/O pins are 5-Volt tolerant? 2. in the Datasheet i reed there is a I/O structure called FT. This structure can tolerate 5V. How VDD_FT in this structure get 5V?
2020-10-15
Re: Hi , I use ST micro controller: STM32H743VIT6 1. I want to knew if the I/O pins are 5-Volt tolerant? 2. in the Datasheet i reed there is a I/O structure called FT. This structure can tolerate 5V. How VDD_FT in this structure get 5V?
2020-10-15
The Input pins of STM32H743VIT6 can tolerate 5V?regards the VDD_FT, if the STM32H743VIT6 doesn't have 5v charge pup how this pin cat have 5V?
Re: Hi , I use ST micro controller: STM32H743VIT6 1. I want to knew if the I/O pins are 5-Volt tolerant? 2. in the Datasheet i reed there is a I/O structure called FT. This structure can tolerate 5V. How VDD_FT in this structure get 5V?
2020-10-15
The Input pins of STM32H743VIT6 can tolerate 5V?regards the VDD_FT, if the STM32H743VIT6 doesn't have 5v charge pup how this pin cat have 5V?