Thank you for your fast response!I have TouchGFX Generator 4.13, 4.14, and 4.15 listed under software packages in CubeIDE. However when I open the .touchgfx file from inside the IDE TouchGFX Designer 4.13 opens. Could this be the issue? It is possibl...
Was the root cause of these vertical lines ever found? I am having the same problem in my project with lines identical to the ones shown here. Hardware is similar to STM32f746G-Discovery, CubeIDE, TouchGFX 4.13
Hello Martin, was the cause of this vertical line artifacts ever found? I am having the same issue with Hardware is similar to STM32f764-Disco, Cube IDE 1.4.2, Touch Designer 1.13.0.Thank you,