I have done the research but couldn't do more than triggering the adc cycle with a timer trigger. Is there any example to do it using cube mx and DMA? Thank you
Okay I see your point now. There is something I didnt understand though, Let's say I chose TIM 5 to be master and the bus it is connected to is 84MHz. So I set its prescaler to zero and counter period to 1000, so I have 84 kHz clock source to TIM1. A...
Thanks for the answer. I am actually doing this without using extra timer by using channel 4 of timer1 in OC mode. This OC event triggers injected conversation. But I couldn't find a way to do it using DMA. Currently I am polling values in Conversati...