Posted on July 13, 2017 at 16:48Have been working with this guys a couple of weeks and the yare asom, but the code seems to be draining power like crasy even in stop mode 1mA.Has any one been able to lower power consumption on stop to uA?
Posted on July 20, 2017 at 17:05 Yes Indead st.mcu I disabled all led configurations and initializations. And fisicaly Conected VDD_TCX0 to PA and changed in mlm32l0xx_hw_conf.h #define RADIO_TCXO_VCC_PORT GPIOA #define RADIO_TCXO_VCC_PIN...
Posted on July 13, 2017 at 19:51 , ,Finaly solve it ,Conected VDD_TCX0 to PA10and changed ,mlm32l0xx_hw_conf.h ♯ define RADIO_TCXO_VCC_PORT GPIOA , ♯ define RADIO_TCXO_VCC_PIN GPIO_PIN_10And worked imidiatly PA12 might have some extra configuration ...
Posted on July 13, 2017 at 19:40I conected TX0 to PA12 and for some reazon it does not Join any more if i conect it to VDD it will conect imidiatly.OTAADevEui= 32-37-38-31-4B-37-7F-03AppEui= 12-34-56-78-9A-BC-DE-FFAppKey= 12 34 56 78 9A BC DE FF 12 ...