Posted on May 12, 2017 at 17:04 Hi; I have stm32f103c8t6 mcu and LSM330 6DOF imu sensor. I try to read from LSM330TR imu sensor. I have a problem. When I read gyro datas from imu, everything is OK. I can read them, but when I tried to read acc ...
Posted on May 25, 2017 at 16:14I share the image of the result I obtained when I observed the i2c communication from the logic analyzer. It's always giving me NAK.
Posted on May 25, 2017 at 14:58I'm going to look with logic analyzer. I checked both of the addresses and the software is returning an Acknowledge Failure Error. Well about this sensor, are there a source code or are there different document from da...
Posted on May 18, 2017 at 13:36Yes,I have and I could share my schematic. If the problem was from the i2c configuration, I do not think I could read gyroscope data or if the problem was from the HW conncetion, it should be in LSM330. In this status,...